Hi,
I have designed a regulator circuit with ADP5071 for 1A load but I need 1.6A load. In board I have two ADP5071 regulators. Both the regulator outputs are 5V and one has 1.4A load and other has 0.2A load.
1. Is it OK, if I connect both the regulator outputs in parallel (by shorting directly both outputs)?
2. If not, please suggest how to do parallel.
Thanks & Regards,
Lakshmaiah S.