Hi, I am designing a 2 phase buck converter,48V to 12V 300W per phase, using the LTC3871 controller and LTpowerCAD. One of the parameters to configure is the current limit via the ILIM pin. In the following picture, the current limit is configured. My question is: the Target Iout Limit on the red circle should be per phase or for the complete converter? It's lools like LTpowerCAD uses the Iout for the complete converter but the datasheet specifies the configuration of this pin using the current per phase.