Post Go back to editing

LTC4234 reverse current protection

Hi team - 

 

I am looking for 12V Hot swap solutions with below features .

  1. Forward current limiting
  2. Reverse current block
  3. Over voltage protection
  4. Over current protection /short circuit protection .
  5. Adjustable current limit  

 

I prefer to use integrated MOSFET solution with forward current limiting & reverse current block .

 

Please let me know if LTC4233 /LTC4234 support reverse current block feature  , It’s not clear to me from the datasheet. 

 I would like to know if reverse current block feature is supported only with  external MOSFET Solutions .

 

LTC4233: https://www.analog.com/media/en/technical-documentation/data-sheets/4233f.pdf

LTC4234: https://www.analog.com/media/en/technical-documentation/data-sheets/4234fa.pdf

Parents
  • Inside LTC4233/34, there is one MOSFET. This MOSFET will do forward current limiting. This will not block the reverse current as body diode of the MOSFET will conduct current in reverse direction. You will have to use an ideal diode part (LTC4410,LTC4412,LTC4376) to achieve reverse current blocking functionality. You can also check LTC4368 which can do forward and reverse over current blocking.

Reply
  • Inside LTC4233/34, there is one MOSFET. This MOSFET will do forward current limiting. This will not block the reverse current as body diode of the MOSFET will conduct current in reverse direction. You will have to use an ideal diode part (LTC4410,LTC4412,LTC4376) to achieve reverse current blocking functionality. You can also check LTC4368 which can do forward and reverse over current blocking.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.