Post Go back to editing

LTC3407-2 Sync Clarification

Is any more information available about using the LTC3407-2 in externally synchronized mode by feeding a clock signal to the MODE/SYNC pin? A general description of the synchronization mechanism would help answer several questions...

Specific questions:

  1. The synchronization frequency f_sync is described as "2.25 MHz typical" in the datasheet, with no minimum or maximum. What is the acceptable synchronization range?
  2. What is the allowable cycle-to-cycle variation in f_sync period? I'm looking at using a LTC6908-1 spread-spectrum oscillator (+/- 10% spreading nominal, 12.5% max); is this acceptable?
  3. I'm used to regulators where external synchronization requires the sync frequency to be faster than the set frequency; for this part, the sync frequency is right in the middle of the set frequency range. How does the part detect the presence of a sync signal, and what is the behavior if the sync signal appears (due to slow oscillator startup) or disappears (due to fault) after the regulator is already operating?
Parents Reply Children
No Data