Post Go back to editing

What precision of output current of the LT3517 in temperature range 10 to 50 Celsius degrees?

Per data sheet (p.9) of the LT3517, when the CTRL pin voltage is less than 1V, the LED current is: ILED =VCTRL/(10*RSENSE).

Question: What precision of this equation in temperature range of +10 to +50 Celsius degrees?

Parents Reply Children
No Data