Post Go back to editing

Problem with ADP3334 at initial startup

Hello Everyone,

I have used ADP3334 to execute power sequencing of adas3023. I have connected the SD pin of ADP3334 to FPGA  so that I can turn its output ON at my desired instant. Unfortunately at initial power up When FPGA is loading its program LDO ADP3334 Turns on and disturbs the power sequencing of ADAS3023. I should have used some active High LDO. But the board is prepared now. Any Help Plz ? Below is the schematic part of adp3334 and snapshot of my signals. Top waveform represents 5V-IN , Middle one is SD input connected to FPGA and 3rd is 3.3V output

.

Edit Notes

Schematic and Wave form attached
[edited by: Asim Malik at 2:07 PM (GMT 0) on 16 Dec 2019]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.