Restrict charging temperature of ADP5062

Hi

I'm using ADP5062 in my product. The battery pack says that its charging temperature should be 0°C-40°C and the battery should not be charged outside that. However, as measured, currently the charging stops at -4.8°C and +58°C, which are quite close, what the data sheet says (0°C - 60°C)

Is it possible to change the the temperatures programmatically or by tweaking the NTC resistor line?

 

This problem is related to tests against standard EN 62368-1, which specifies that the battery shall not be charged at a temperatures outside the temperature specified the battery manufacturer.