Hi,
I'm currently having an output issue that I hope someone can shed some light on.
I have the LT3094 connected with the following:
GND: pins 6 (ILIM), 9 (GND)
VIN (@ -15V): pins 1 (IN), 2 (IN), 3 (EN/UV), 5 (PGFB), and 13 (Exposed Pad)
PG: NC (floating)
VOUT: pins 10, 11, 12
VIOC: NC (floating)
SET: pin 8 is set to 130.5kohm (for -13.5V Vout)
** all recommended caps are also in place **
Please see the LTSPice picture. According to ltspice output as well as the datasheet pin definitions and connection info, I was expecting to see -13.5V on my lab circuit.
However, what I'm measuring is -5.999V (-6V) at Vout(?).
There is no overheating of the IC - my only guess/possibility is that the thermal shutdown is tripping.
Suggestions?
Thank you.
RW.