Post Go back to editing

LT4363 LTSpice Model shows current pulse from GATE pin to GND pin in IEC 61000-4-5 8/20us 2kV/1kA test

Hello,

attached data is an LTSpice model test setup of LT4363-2 based cirquit, exposed to IEC 61000-4-5 8/20us 2kV/1kA pulse.

 LT4363-2_IEC.zip

Simulation data demonstrates a considerable current pulse from GATE pin to GND pin of LT4363 immediately after surge onset, for which no valid path exist as per datasheet block diagram. In 1us a normal pulse starts from GATE pin to SNS pin, evidently due to current fault, which seems to terminate the pulse to GND pin.

Is it an intended behavior?

Regards,

Sergey

Parents Reply Children
No Data