Post Go back to editing

ADP2386 footprint

While making a footprint for ADP2386 i have notice, that dimentions in datasheet is wrong

IC side max - 4.1 mm

Pin length max - 0.5 mm

Exp pad max width - 1.5 and 1.05 mm

Pad to pins min gap - 0.2 mm

Pad to pad min gap - 0.45

Make some calculations: 0.5*2+1.5+1.05+0.2*2+0.45=4.4mm

If i place pins in acording to JDEC, gap between pins and exp pads being around 0.05mm, it's impossible

Any suggestions? Maybe official tech support could explain it?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.