Post Go back to editing

LTC3637

Hi,

We are using LTC3637 to generate +12v to -12v as per the typical application diagram given in datasheet pg no 21.

Usually we will connect EXPOSED PAD of IC to ground, but in our case output(-12v), is taken from the ground pin. According to datasheet pg no 8, exposed pad (pin no 17) is connected with gnd (pin no 8) so we have to connect  exposed pad also to output(-12v).

Our concern is, if IC will be able to withstand the thermal extremes or not , since exposed pad cannot be grounded and is to be connected to -12V?

Shyama

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.