To whom may it concern.
Hi I'm HS.
I have DC2476A-A and want to use T2P as type indicator via LEDs, which means I want to use 3 LEDs so that they indicate 4 states: af, at, bt(around 61W), bt(around 71W)
I set the output as 28V.
If I attach the LEDs to the secondary part of octo-coupler, LEDs will be oscillating from V_OUT=28V to 0V so it may make users frowned upon or seem to be stagnant since Pin T2P throw pulses out to octo-coupler at 976Hz.
So my question is...
1. What would be the most effective way to indicate 4 states using LEDs?
2. Is there any specific action when PD is demoted so that you can tell it is demoted or just normal operation.
ex) Datasheet said, 50% 976hz pulse means 51W --> Class 6.
How do you know if it's normal operation(class 6 by itself) or it is demoted?
3.
3-1. I want to change the voltage level of the T2P pulse cuz it's too high(Since V_OUT=28V) to connect to LEDs
Would it be ok if I pull-up to other voltage values, somewhat lower than V_OUT(=24V)?
Or How can I lower the voltage value in addition to connecting resistors in series with pull-up resistors?
3-2. I think i may attach LC filter to T2P so that it alters pulse into a smoothly-filtered continuous voltage waveform, DC. 3 comparators which are made of op-amps will be placed next to the LC filter. I hope the output of comparators is around 1.8V. I think I draw 1.8V from somewhere, idk..maybe voltage regulator from 7805 or something, and connect it to VDD of comparator.
Do you think it's a good idea to discern the state of PD(af,at,bt) and send this data/signal to end- device??
3-2-2. Comparator's VCC and V_REFs will be given/divided by V_OUT. V_REF will be referenced from V_OUT via 5.1V Zener Diode. Do you think it's a good way to get VCC from secondary area?
4.
4-1. What's the purpose of R13, C17 on the primary side of T3 and C20, D13, R18, R15 on the secondary side?
4-2. Reference schematic put zener diode, D17(PMEG1020EA) at Pin PG , but no zener at Pin SG. What's the difference??
4-3. Reference schematic put gate driver at secondary power MOSFET but nothing at primary power MOSFET. What's the difference??
4-4 Why does gate driver need Transformer(T3)?, Why didn't reference design connect gate driver to Pin SG directly??
5. In reference schematic, Output filter has R35(Opt). What effect can we expect if we insert this R35? Any voltage drop? Higher filter performance??
6. In reference schematic, R5(8.2Ohm) is connected to Pin VPORT in LT4295. What's the purpose of this R5?
7. This is the screenshot of PoE ideal MOSFET Diode Bridge using LT4321 in DC2476A-A
What's the purpose of R28, D2, D3 and C11??
8. Layout.
I couldn't find any information/tips for layout of DC2476A-A.
Is there anything that i have to know and take care of when it comes to layout??
I think you guys use 6 layers PCB.
What's the impedance of pcb and what width should i use for line and data??
Thank you for your hard work and I appreciate it a lot
Hope you have a good day
1. The T2P pin uses duty-cycle to encode the physical layer classification result, which is how much power the PD has been allocated. This means you only need to use a single opto-coupler to send this information…
Hi, Eric.
Thank you for your detailed information and explanation!
I really appreciate it a lot!
These screenshots are the T2P + LC filter + Comparator + LED and 5.1V Zener + Voltage divider.
1-1…
Hey HS,
1. I would use the Zener + NPN to generate the 5V1 so you don’t have to worry as much about loading the 5.1V rail. A resistor and Zener always burns power and has poor load regulation. The…
1. The T2P pin uses duty-cycle to encode the physical layer classification result, which is how much power the PD has been allocated. This means you only need to use a single opto-coupler to send this information across the isolation barrier. A microprocessor is the simplest way to decode this information. This only requires a single digital input and a couple lines of code.
2. You know if the PD is demoted by comparing the PD’s Requested Class (i.e. what resistors are installed at the CLASS and CLASS++ pins) and the T2P signal. Requested Class is determined when you build the PD, it does not change. If you see T2P with a 50% 976Hz pulse, the PD has been demoted if it is Class 7 or Class 8, but it has received full power if it’s Class 5 or Class 6. For example, see Table 5 in the datasheet. A Class 6 PD has four T2P states. They correlate with Demoted to 13W, Demoted to 25.5W, Received Requested 51W, and operating with Auxiliary Power.
3-1. Yes, you can use a lower voltage to drive the opto-coupler’s collector. 24V is used on this board because that is the output voltage. The opto-coupler supply can easily be lower; 3.3V and 5V are commonly used. I recommend using a resistor / BJT / Zener regulator for a quick and cheap low voltage, low current supply. An linear regulator is another option.
3-2. The downstream circuitry should know the T2P result, so it can reduce the load if the PD has been demoted. If a PD doesn’t implement demotion it may be disconnected by the PSE when it draws too much power. As I mentioned earlier, it is quite trivial for any microprocessor to detect a digital duty cycle. An averaged (LC filtered) T2P signal can also be measured with an ADC. Using comparators is another good option. You could also use a window comparator to detect if the average T2P signal is at 50%, etc.
3-2-2. I don’t see the Zener in the schematic you shared. Please see the earlier comment about using a Zener and BJT to generate a low voltage bias rail. I also recommend you simulate your LC filter and comparator circuit using LTSpice.
4-1. These components form an undamped L-C circuit for the isolated secondary-side gate driver signal. I do not recommend changing these values.
4-2. This is a Schottky diode, not zener. I recommend BAT54WS for new designs. The SG pin does not need a diode.
4-3. A gate driver is needed on the secondary because the gate drive signal should be refreshed after crossing the isolation barrier.
4-4. The secondary-side needs to be isolated per IEEE, to 1500VRMS.
5. This resistor optionally damps the output filter, as the inductor affects the control loop. This resistor would allow us to bypass the filter or modify the filter response for different designs. You can ignore it for your design.
6. This resistor is optional and improves performance.
7. C11 locally biases the LT4321, D2 provides protection, R28 allows you to optionally use /EN and D3 enables the bridge after classification.
8. Please use the DC2476A-A as a guideline for the layout. Follow the standard rules for a flyback or isolated converter layout. DC2476A-A is a 6-layer board, but the design could modified for a 4-layer board, perhaps even a two layer with some care. Please keep the data + power traces as short as possible and size correctly for current capacity. These are the traces between the RJ-45 and ethernet transformer. The data traces that come from the ethernet transformer are differential pairs. Each pair should have a differential characteristic impedance of 100 Ohms. I recommend you follow the guidelines provided by your PHY manufacturer.
Best Regards,
Eric
1-1. This voltage divider is set by 5.25k, 1.4k, 3k, 1k. Wouldn't it be too heavy for load??
1-2. Which one would be better, the one you recommended me to or the one i did and why is it so?
2. You mentioned R5 is optional and improves performance. What kind of performance do you mean and how?
3. You mentioned C11 locally biases the LT4321 tho, if you don't mind, would you break it down little bit more that i can understand??
4. Which component would be taken care of when you do layout with regard to thermal analysis??
Would you give me advice on thermal design? Like..do you need thermal pad or something when you use the board as class 8 PD?
5. I assume I need to change the value of the R25(20k) if I change the V_OUT which is applied to opto-coupler to V_REF=5.1V. What would be the ideal value? Also, is there any replacement for this opto-coupler? Because it's kind of old components, I think, So if i change it to the latest model, I might improve the efficiency or thermal effect.
Thank you for your hard work again.
All the best
1. I would use the Zener + NPN to generate the 5V1 so you don’t have to worry as much about loading the 5.1V rail. A resistor and Zener always burns power and has poor load regulation. The circuit I recommended only burns power when current is drawn from the output. The load regulation is much better, and it can source more current, as long as the BJT can handle the power dissipation.
2. As for R5, I'm talking about the about the control loop. The output capacitor and inductor will affect the gain margin and phase margin.
3. It’s recommended that you locally bias most ICs, this means place a capacitor near the pins so that there is a low impedance path for current transients. LT4321 doesn't require much capacitance, only 47nF is recommended.
4. Most of the heat will be in the primary and secondary MOSFETs, primary and secondary snubbers, and the transformer. You should make sure there is enough spacing around the snubbers and FETs as they will be the warmest components. Here is a thermograph of the this demoboard.
5. Any off-the-shelf optocoupler should work. It does not need to be particularly fast, it just needs to support a few milliamps and withstand your output voltage. I would recommend one that has a Current Transfer Ratio (CTR) that is 150% - 300%, instead of a wider range like 100% - 400% or 80% - 600%.
I recommend you modify your circuit to use the BJT / Zener to supply the Opto-coupler and comparators such as ADCMP393, as well as a resistor divider to provide references. I would only have indicators for Power, 25.5W, 51W, and 71.3W. I would recommend a window comparator, and I can share this idea with you over email.