Post Go back to editing

LTC3859 - pcb reference design

Thread Summary

The user encountered issues with Vout3 blowing up when Vout2 is under load while designing a PCB based on Figure 15 of the LTC3859A datasheet. The final answer suggests checking the PCB layout to ensure switching nodes and gate drive traces are not routed near sensitive pins like ITH, FB, SS, FREQ, and MODE. The reference design files for the LTC3859A evaluation board are available for download.
AI Generated Content

Hi,

Could you share with pcb reference design please?

As I do not found eval board for this IC I design pcb. Unfortunately looks like I did something wrong because load on Vout2 makes channel Vout3 blow up (if also under load).

So only Vout1 and Vout2 or Vout1 and Vout3 can work in same time.


I used your circuit Figure 15. High Efficiency 1.2V/3.3V Step-Down Converter with 10.5V SEPIC Converter.

Thanks SLA