LT8390 and LT8490

Hi,

I understand that there currently is not a model for the LT8490 that has been made yet? However, I am trying to simulate an MPPT but instead of using the LT8490 in the LTSPICE model I wanted to use the LT8390 as that is an available model. However, in the LT8390 datasheet, it says it is possible to have an output from 1-60V the example on page 32 of the data-sheet is for 125W (25V 5A) Solar Panel to 12V Battery Charger, What parameters must be changed to change the output voltage to a different voltage such as 36V or 40V? Is it also possible to connect a solar cell as the input into the system?

Parents Reply Children
No Data