Post Go back to editing

LTC3624 - external SYNC clock signal

I am designing power supply for my project using LTC3624 in the Force Continuous Mode.

The datasheet is indicating the “SYNC signal to a voltage between 1V and VINTVCC – 1.2V for forced continuous mode. Furthermore, connecting MODE/SYNC to an external clock will SYNC the system clock to the external clock and put the part in forced continuous mode.”, however the using the LTspice and model provided in LTC3624_DC2005A_TA01A and LTC3624_DC2359A the device does not run in Force Continuous Mode.

For the simulation of the LTC3624 to run in Force Continuous Mode the external SYNC clock signal control voltage, need to be lower than the 0.7V.

What is external SYNC clock signal recommended the minimum and maximum voltage?

Thank you,

Mihail