KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
LTC3786
Production
The LTC3786 is a high performance synchronous boost converter controller that drives all N-channel power MOSFETs. Synchronous rectification increases efficiency...
Datasheet
LTC3786 on Analog.com
LTC1754
Production
The LTC1754 is a micropower charge pump DC/DC converter that produces a regulated output. The input voltage range is 2V to 4.4V for 3.3V output and 2.7V...
Datasheet
LTC1754 on Analog.com
Hi EngineerZone community,
I'm designing a li-po battery booster with LPC3786 which is able to convert 3-4.2V battery voltage to 18V 5A, for this purpose I tried to customized one of the sample circuits from the datasheet, (3786 F13a ) I have changed a few of components and entered the values in the LTpowerCAD project file and it seems to work, the only problem I can see is that as the original sample circuit's output voltage is 5V the output of the circuit is connected to the output pin of the LTC1754 pin (through the body diode of mosfet Q), which has the maximum rate 6V of the pin voltage so now with the output voltage of 18V is there any other solution for that ? maybe just replacing mosfet with a simple diod ?
is there any other problem you can mention in the circuts ?