KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
LTC3786
Production
The LTC3786 is a high performance synchronous boost converter controller that drives all N-channel power MOSFETs. Synchronous rectification increases efficiency...
Datasheet
LTC3786 on Analog.com
LTC1754
Production
The LTC1754 is a micropower charge pump DC/DC converter that produces a regulated output. The input voltage range is 2V to 4.4V for 3.3V output and 2.7V...
Datasheet
LTC1754 on Analog.com
Hi EngineerZone community,
I'm designing a li-po battery booster with LPC3786 which is able to convert 3-4.2V battery voltage to 18V 5A, for this purpose I tried to customized one of the sample circuits from the datasheet, (3786 F13a ) I have changed a few of components and entered the values in the LTpowerCAD project file and it seems to work, the only problem I can see is that as the original sample circuit's output voltage is 5V the output of the circuit is connected to the output pin of the LTC1754 pin (through the body diode of mosfet Q), which has the maximum rate 6V of the pin voltage so now with the output voltage of 18V is there any other solution for that ? maybe just replacing mosfet with a simple diod ?
is there any other problem you can mention in the circuts ?


Hi, the major problem that you would encounter here is that the output voltage limit of LTC1754-5 is only 6V. Putting an 18V across it would damage this IC. This suggested circuit in page 28 is designed for a lower Iq and low output voltage. Do you really need a lower Iq that's why you are attempting to use it? Maybe using the circuit you obtained from LTpowerCAD is enough.
Regards,
Hi. one possible solution is to directly connect the Vout of LTC1754-5 to Vbias and remove D2. Hence, the Vbias will always come from LTC1754-5. By the way, may I know what company are you from? May I also know your estimated amount of usage (EAU)?
Regards,
directly connecting the Vout of LTC1754-5 to Vbias doesn't affect the efficiency on higher output voltages ? actually I think this is a solution for low input voltage not low Iq,
I wan't to use this circuit on a free and open source project.
It is a solution for low input voltage. Low Iq in a sense that VBIAS will come from 5V after PGOOD is ok which is close to minimum requirement.
Make sure that output current of charge pump is enough to provide for VIAS pin.
It is a solution for low input voltage. Low Iq in a sense that VBIAS will come from 5V after PGOOD is ok which is close to minimum requirement.
Make sure that output current of charge pump is enough to provide for VIAS pin.