Hi,
we have a requirement to design Buck-Boost converter which takes 2.5V to 12V as input and generates 3.3V @ 1A to 2A.
This has 2 scenarios of operation.
Scenario1:
default mode:
Input voltage : 10.8 to 12.6V, Typ-12V
Output: 3.3V @ 1A rare peaks 2A
Scenario 2 :
When main power lost auxillary power comes to the Input
Input voltage : 2.5V to 5.5V- Typ is 4.6V.
Output : 3.3V @ 1A
I see LTC3112 suits well to this application.
I couldn't able to find LTSpice application circuit for quick validation.
Here are my questions:
1. Is this suitable device for this input range? if not suggest alternate
2. I see Output current is dependent on duty cycle in boost mode - I need data on at what input voltage in this range (2.5V to 5.4V), LTC3112 can supply max load current and how much is the ~current.
3. If you can provide a LTSpice circuit - it will be helpful for quick check. I tried to change the values in demo circuit but without success