Hi,
Would you let me know how to connect the MODE, MIN, DIM and VT pin on ADP8140CP-EVALZ when the board is set to PWM dimming mode using VT pin?
The current setting on the board is as follows:
- MODE pin is connected to REG
- MIN pin is connected to REG
- VT pin is connected to PWM signal (0 and 3.3V) which is generated by my custom board.
- DIM pin is open.
This setting did not work at all. there are no description on the datasheet how to use PWM mode with VT pin in detail.
It worked when the board was set to PWM mode with DIM pin. However, P-ch MOSFET became too hot ( it read around 80 C deg on case).
To prevent this heat condition, I' d like to apply a PWM current sink mode with using VT pin (I'm not sure how to call).
I'm wondering if the board does not work as a PWM mode with VT pin on ADP8140CP-EVAL.
Please let me know if I'm missing anything about pin setting on ADP8140CP-EVAL.
Regards,
ytak