Hello,
we use ADP5061ACBZ-5-R7.
If device is configured via I²C, charge is complete after configured termination voltage in adress 0x03 is reached. That's the expected behavior.
If device is unconfigured, the device works with Default Termination voltage ( 4,20V ).
After Charge complete ( 0x0B=4C ) the current stops for t(end)= 7,5min.
After this time, a current of ~260µA charges the battery unexpectedly. If I start our controller, current increases to 1,2mA.
I recognized this behavior on 3 pcbs.
Any idea ?
Best regards,
Drostec
Edit Notes
tagged[edited by: JValeriani at 7:38 PM (GMT 0) on 9 Oct 2019]