Post Go back to editing

LTM8055 Parallel Operation

Hello,

I have a few questions about the LTM8055.  The LTSPICE demo circuit for parallel LTM8055  found here https://www.analog.com/en/products/ltm8055.html#product-tools shows a large voltage overshoot on startup and very high current demands from the modules.  Is this realistic of the modules in a parallel configuration or is this a simulation artifact?  The datasheet doesn't mention anything about parallel startup being a problem.   The single device LTSPICE model doesn't have this problem.  The simulation is for a 12V output and the voltage goes to almost 24V before settling.

Unrelated to the simulation, does the device have short circuit protection in all modes of operation (buck and boost)?  Do I need to do anything special for parallel devices for fault protection?  Do they have any circulating problems during faults?

Parents
    • Hi, I also see an overshoot in my simulation, I suspect that this is due to imperfection of the LTSpice model. Let me verify this in bench and I'll get back to you as soon I get the result. 
    • As for your other questions, it is stated in page 9 of the data sheet that "an output sense resistor is required to adequately protect the LTM8055/LTM8055-1 against output overload or short-circuit". This is applicable in all modes of operation of the LTM8055.
    • Kindly refer to page 11 of the datasheet if you are going to use this in parallel operation. Additional fault protection may be required as stated in page 14 when the input voltage rises above a predetermined threshold due to some applications where the FB pin is abruptly driven to a new voltage.

    Regards, 

    Fritz

Reply
    • Hi, I also see an overshoot in my simulation, I suspect that this is due to imperfection of the LTSpice model. Let me verify this in bench and I'll get back to you as soon I get the result. 
    • As for your other questions, it is stated in page 9 of the data sheet that "an output sense resistor is required to adequately protect the LTM8055/LTM8055-1 against output overload or short-circuit". This is applicable in all modes of operation of the LTM8055.
    • Kindly refer to page 11 of the datasheet if you are going to use this in parallel operation. Additional fault protection may be required as stated in page 14 when the input voltage rises above a predetermined threshold due to some applications where the FB pin is abruptly driven to a new voltage.

    Regards, 

    Fritz

Children