Post Go back to editing

Rewriting PSM when using LTM4686 in parallel drive

I have the following concerns about using LTM4686, please let me know

The LTM4686 is planned to be used in 4-parallel to drive 0.6V to the MCU.


Pin-strapresistors configure start-upsettings(output voltage, register address, phase, etc)

Since I want to change the output voltage according to the load, 
I2C communication is performed from the MCU and the LTM4686 setting is changed 
so that the register value is read from the resistance value.
At this time, the address and rail address are also changed.

Since the voltage is applied to the MCU from the LTM4686, there are the following concerns.
Will the output voltage be reset when the register is rewritten?
(I am worried that the LTM4686 will not be reset by changing the address)

Parents
  • Hello, 

    Resistor configuration externally can set the output voltage and phases at start up.

    Once LTM4686 are started, the output voltage can be changed via VOUT_COMMAND register at any time. 

    If rail address MFR_RAIL_ADDRESS is required to be changed online, it will not affect the rest of the register values. 

    Regarding for MFR_ADDRESS, 4 LSB address is decided by the external resistor at ASEL pin and 4 MSB address is decided by the value stored in NVM. For instance, default MFR_ADDRESS is set as 0x4F. When selecting the 1.65K resistor from table 5 from datasheet page 48, the address for this module will be 0x42. As  LSB address is decided by resistor, this LSB value won't be changes via software.

    Thank you.  

Reply
  • Hello, 

    Resistor configuration externally can set the output voltage and phases at start up.

    Once LTM4686 are started, the output voltage can be changed via VOUT_COMMAND register at any time. 

    If rail address MFR_RAIL_ADDRESS is required to be changed online, it will not affect the rest of the register values. 

    Regarding for MFR_ADDRESS, 4 LSB address is decided by the external resistor at ASEL pin and 4 MSB address is decided by the value stored in NVM. For instance, default MFR_ADDRESS is set as 0x4F. When selecting the 1.65K resistor from table 5 from datasheet page 48, the address for this module will be 0x42. As  LSB address is decided by resistor, this LSB value won't be changes via software.

    Thank you.  

Children