Post Go back to editing

LT3750 - using at constant frequency

Hello,

I'd like to use the LT3750 to charge a capacitor using a specific transformer which requires a 100kHz frequency.

As this controller doesn't have the ability to configure the frequency - is there a way to do it using one of the pins. Now the frequency varies between 30kHz to 150kHz while I'm using the controller.

Otherwise, is there an alternative to this controller (capacitor charger) which has a way to configure the frequency?

Thanks

Parents Reply Children
No Data