Hi,
I have a few questions about the LTM8054.
There was also a slight device heat generation.


The same symptom does not occur while using it now.
Is there any countermeasure for each device?
I would appreciate your answer.
Best Regards.
Hi,
I have a few questions about the LTM8054.
I would appreciate your answer.
Best Regards.
Hi I'm an FAE working closely with the questioner. By what is described in his question it looks FCM accidentally kicks in when not usingthe 0.01uF cap?. I myself could not find clear expalation on the nesessity of the cap, or the difference in terms of the cap between the circuits appear in pate 23 and 24 in the datasheet . Woudl you be able to help out? Also, They are worrying the same applies to the LTM8055.
Hi
On page 16 under "Switching mode" of LTM8054 datasheet, When mode and LL are connected together it is actually suggested to add ~0.1µF between this pins and ground to improve the light load transient response by delaying the transition from the discontinuous to forced continuous switching modes.
This is the same with LTM8055
Regards,