Hello,
I willing to imlement PSU with buck converter with LT3088 LDO and looking at example in datasheet p26 I see one portion of circuit which is of unclear function. Could someone explain what it does and how it works?

LT3088
Recommended for New Designs
The LT3088 is an 800mA low dropout linear regulator designed for rugged industrial applications. A key feature of the IC is the extended safe operating...
Datasheet
LT3088 on Analog.com
LT3680
Production
The LT3680 is an adjustable frequency (200kHz to 2.4MHz) monolithic buck switching regulator that accepts input voltages up to 36V. A high efficiency 95mÎ...
Datasheet
LT3680 on Analog.com
Hello,
I willing to imlement PSU with buck converter with LT3088 LDO and looking at example in datasheet p26 I see one portion of circuit which is of unclear function. Could someone explain what it does and how it works?

That part makes a negative voltage rail that allows the LT3088 output adjustment to go all the way down to 0V.
The LT3088 has a minimum load of around 2mA, so the LT3088’s output will never go to 0V unless there is a pull-down to a negative voltage.