Hello,
I am working on a design which uses sevral low noise op amps (AD8671) for handling analog signals. I would like some help with choosing a suitable way to power the circuit.
I have an input power supply of 9V DC, and would like to generate +12V and -12V rails. I need these rails to have a ground that is galvanically isolated from the input 9V power supply. I also require the output voltage noise to be below 100 uV rms (in a bandwidth up to several hundred kilohertz).
I was thinking that the best way to achieve this would be to have an isolating DCDC converter, followed by positive and negtaive low dropout regulators, but am open to suggestions. Would someone be able to recommend some options for a combination of parts that can provide the +12V and -12V rails I require?
Thank you!