Post Go back to editing

LTC3111 Boost

 I am using the LTC3111 as a 7V boost and need at least an output of 700mA @ 7V. Whenever more than about 350mA is pulled from the device, output voltage drops, and when even more current is demanded of the device, the power output becomes unstable and drops out. When the boost is stable, the device is switching at the correct frequency, however, as more than 350mA is demanded of the boost, the switching frequency drops off. Any suggestions are appreciated, I'm not sure where to go at this point as I have been through the data sheet multiple times.