Post Go back to editing

Maximum sink current of PG pin for LT3045

Thread Summary

The user inquired about the maximum sink current of the PG pin when it is in the POWER not GOOD state. The final answer specified that the pull-down current should not exceed 100uA. An accompanying answer noted that with a 12V input and a 200kOhm resistor, the current at the PG pin is approximately 60uA, which is within the safe limit for a CMOS input logic.
AI Generated Content

What's the maximum sink current of PG pin when it is pulled low internal (POWER not GOOD state)?

Thanks

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.