Hi I am confused with the explanation regarding some of the calculations for the Boost topology on page 15 of the data sheet for the LT8711.
Please walk me through the step 2 and 3 . Also please define for me the units of DC max and how it relates to the graph on page 5 with the following example...
Min Input voltage 23.8V
Max Input voltage 24.2V
Vout 29 to 30 volts
Output current 3 Amps
Regards
Dave