| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. | Open | |
LTC7862
Recommended for New Designs
The LTC7862 high efficiency switching surge stopper protects loads from high voltage transients. High efficiency switching allows high output currents...
Datasheet
LTC7862 on Analog.com
LTC7860
Recommended for New Designs
The LTC7860 high efficiency surge stopper protects loads from high voltage transients. High efficiency permits higher currents and smaller solution sizes...
Datasheet
LTC7860 on Analog.com
HI ADI Expert,
We would like use LTC786x as surge stopper and it need pass MIL-STD-1275D standard.
We picked LTC7860 first but we can't find 250V P-MOS with low RDson so Power dissipation is quote large.
Now we're studying LTC7862 which use N-MOS, but we can't find description about designing with floating ground. ( It describes very clearly in LTC7860's datasheet )
May I know :
1. Does ADI provide LTC7862 reference design which pass MIL-STD-1275D standard?
2. Can you share more design note about designing LTC7862 with floating ground?
Thank you!
At this time, ADI does not have a MIL-STD-1275D LTC7862 reference design. The input voltage of the LTC7862 is limited to 140V which will accommodate the 100V surge requirement, but not the 250V, 15mJ spike requirement. While it is likely possible to extend the input range of the LTC7862 with the use of a high-side driver (and bias supply), the N-Channel LTC7862 does not support the floating ground configuration used with the LTC7860.
Hi Kurk. If I would like to increase the input protection for, say, a voltage spike of 600V and perhaps other fast transients such as lightning, will adding a TVS diode improve the protection?
I do not have any direct experience with the 600V spike requirement but I see that an optional TVS is shown in the article titled High Voltage Surge Stoppers Ease MIL-STD-1275D
Compliance by Replacing Bulky Passive Components https://www.analog.com/media/en/technical-documentation/tech-articles/lt-journal-article/LTJournal-V24N1-03-df-SurgeStopperMilSpec-DanEddleman.pdf . Guessing some impedance (EMI filter, etc.) would proceed this circuit but not sure.
I do not have any direct experience with the 600V spike requirement but I see that an optional TVS is shown in the article titled High Voltage Surge Stoppers Ease MIL-STD-1275D
Compliance by Replacing Bulky Passive Components https://www.analog.com/media/en/technical-documentation/tech-articles/lt-journal-article/LTJournal-V24N1-03-df-SurgeStopperMilSpec-DanEddleman.pdf . Guessing some impedance (EMI filter, etc.) would proceed this circuit but not sure.
I see. Thank you very much for the journal share. Will definitely look into it