LTM4650 Vout sense issue

Dear Sir 

The following test question is customer response

1. Spec p26 circuit  , 

VOUT SENSE connection is not the same as EV KIT Application note (EV Kit part number DC2378A-B )

    

2. Customer demand is that both sets of output must have VOUT Sense(How to set up on the EV Kit)

     Or he can only have one vout with sense function

3. The current customer test results are as follows:
    (1) Vout sense is added to vout 1 and its sense to the loader header is Vout 1=0.943V
         Vout 2= 0.93V with 13mV difference