capacitance of SYNC pin of LTM4646 and LTM4622

Hi there,

we use 10 pcs of  LTM4646 and 10 pcs of LTM4622 on a big power system. System requires External Synchronization Clock (800KHZ) for all DC/DC.

Now ONLY ONE sync clock 800KHZ is generated from FPGA, and feed to 20 DC/DC in daisy-chain topology. The output current driving strength of FPGA pins is about only 4mA, we are not sure whether it is enough to drive so many DC/DC sync pins.

So we hope to know the pin capacitance of SYNC pin (pin.F3 of LTM4646 and pin.C4) , and we can confirm the total load-capacitance, then decide wehter a buffer IC should be inserted.

Thanks.

Top Replies

Parents
  • 0
    •  Analog Employees 
    on Jun 19, 2019 10:21 PM

    The input resistance of the Mode_PLLIN pin for LTM4646 is 600kOhm. 4mA should be enough to drive 20 uModules. For 800kHz switching frequency, input capacitance of the model_PLLIN pins should not be an issue. We don't recommend daisy chain 20 uModules. Usually for daisy chain uModules, the clocking signals for 1st to 4th are pretty clean, but above 4th, the clocking signal starts to have jittering issues.

Reply
  • 0
    •  Analog Employees 
    on Jun 19, 2019 10:21 PM

    The input resistance of the Mode_PLLIN pin for LTM4646 is 600kOhm. 4mA should be enough to drive 20 uModules. For 800kHz switching frequency, input capacitance of the model_PLLIN pins should not be an issue. We don't recommend daisy chain 20 uModules. Usually for daisy chain uModules, the clocking signals for 1st to 4th are pretty clean, but above 4th, the clocking signal starts to have jittering issues.

Children