Post Go back to editing

Short circuit protection on boost dc/dc converter LT1680 based

Hi everyone,

I'm designing a boost dc/dc converter from 12 V to 48 V  5 Ampere

I'm thinking of using a LT1680, would I protect the exit from the short circuit, kindly any suggestions?

Thanks in advance

SPAXIO

Parents Reply Children
  • Hi W.G.

    Many Thanks for the suggestion,

    I think that for my project I will use LT8390,

    I downloaded the simulation file LT8390_DC2431A of evaluation board from from site and I modified the feedback resistor and current sense resistor value to obtain 48V max 5A, also I changed the mosfets with 2 millohms 60 V VDS models, but maybe I can leave in input models with 1 milliohms and 25V on VDS?

    Any other suggestions?

    I attach the simulation schematic

    Best Regards

    SPAXIO