Hi,
I would like to use LT3475.
So, I have a question. Please help me.
Question:
I want to use the LT3475 with 3A output.
However, there is no description other than the circuit example, and the design has stopped.
I want to light the LED at intervals of a few microseconds,
but I think that it is necessary to build a circuit like D/S p.15 to do that.
https://www.analog.com/media/en/technical-documentation/data-sheets/3475fb.pdf#page=15
Even if the same PWM signal is input to PWM1 and PWM2,
"Jitter occurs in the pulse output of the LED current, making it difficult to pulsate the LED in a few microseconds."
Is such a phenomenon likely to occur?
It seems that LTspice is working properly.
Best Regards,
Naohisa.