Hello,
We are using the LTC2953-1 as a switch without a MCU to control a DCDC Converter, the board does get warm and as a safety factor we are to implement a thermal switch off.
I was thinking of using something from the Analog line like the and connecting it to the KILL pin 3 of the LTC2953-1.
It says that the KILL pin has an internal timer of 512ms. Would this mean that connecting ADT6401 output (pin 6) to KILL (pin 3) with a pull-up resistor at 3.3V?
Also, we are going to tie for the future an MCU to the KILL pin too, would it work with both together? When one or the other is tripped the LTC2953-1 is switched off?
I've put attached a simple image to give you an idea what I mean.

I hope to hear from you soon.