Post Go back to editing

LTC 3705 auxiliary supply - lockup on startup

Thread Summary

The user is experiencing an LTC3705 lockup at startup when the supply voltage rises too slowly, potentially due to trickle charge mode. The final answer suggests that the chip requires NDRV - Vcc >= 1.3V and 50uA into NDRV to stay in normal mode. The user has implemented a workaround by adding a 3.3k resistor from 24V to 12V_SR, which lifts the 12V_SR to 14V when the LTC3705 is locked up, allowing it to start switching normally.
AI Generated Content

Hi,

I have a legacy design using the LTC3705. The LTC3705 locks up at startup when the supply voltage rises too slowly. I can replicate the problem by setting the current limit on my lab power very low. After a while I will then increase the current limit, but the LTC3705 stays locked with no switching on the gate outputs. I think the problem may be related to trickle charge mode.

Question:

How do the LTC3705 detect "trickle charge mode? From the block diagram it seems that trickle charge is mode is selected when VCC > (NDRV-0.6V). In our application VCC is supplied from a 12V linear regulator. Since VGDUV is 13.4V in trickle charge mode we want to avoid this mode. To stay in normal mode, this would require VCC < (NDRV-0.6V). In our application this equals NDRV > 12.6V. I measure 12.0V at the NDRV pin. This makes sense if the chip is pulling NDRV low to turn off the external nmos transistor. This again explains why the chip is "dead".

Have I understood this correctly?

Do you have a suggestion on how to force the chip to not be in trickle charge mode?

  • To stay in normal mode, the LTC3705 is looking for approximately >= 1.3V from NDRV to Vcc (meaning NDRV - Vcc >= 1.3V) and 50uA into NDRV.

  • Thanks for the reply. I tried lovering the resistance of R48 to 27k. I measure 12.2V at NDRV when I do this (VCC is 12.02V). I think this is caused by driver for the linear regulator. It is trying to turn off the external NMOS because the voltage is higher than 8V. The current into NDRV is (24-12)/27k=444uA. This problem seems to be biting its own tail. The chip is waiting for the voltage to rise to 13.4V while at the same time it is driving NDRV low as long as the voltage is >8V? Any suggestions are welcome.

  • The majority of the applications appear to use a "standard 3V threshold type (i.e. not logic level)" MOSFET. Page 18 of the LTC3725 Data Sheet shows another option (which may or may not have the same problem as you already have - I am not sure.) Where is your 12V coming from (and when with respect to the input voltage)? What is the input range? Depending on this information, I would think a variation of the standard MOSFET solution is the best bet.

  • Thanks. The 12V is coming from an LM317 regulator. The answer to "when" depends on the rise time of the input 24V feeding both the lm317 and the LTC3705. I agree that it was a dumb decision to not use the standard MOSFET solution on this board. The problem is that we have a number of boards in the field and some of them are failing when the 24V feeding the board is connected to another board with a heavy capacitor bank. When the 24V rises very slowly, the LTC3705 locks up. I have sort of solved the problem by fitting a 3.3k resistor from 24V to 12V_SR that lifts the 12V_SR to 14V when the LTC3705 is locked up. When the LTC3705 then starts switching it consumes more power and the 12V_SR drops to 12V again. It's a small hack but it gets around the problem. If there is a more elegant solution that I could retrofit to these boards please let me know.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.