LT3065 PWRGD

The PWRGD signal on the LT3065 stay high when the SHDN pin is low, where the datasheet state that it should remain low if the output is less than 90% of the nominal output value. 

When the SHDN pin is set to high, the PWRGD pin will pulse low for 3 ms and then return to high.  PWRGD pins detects fault like current limit but doesn't reflect the output status which is not good for power sequencing.

It is a known issue for that device?

NOTE : We have tested the LT3065IDD#PBF


Thanks.

Parents Reply Children
No Data