Post Go back to editing

About ADP1613 COMP pin absolute maximum rating

Hi

I have a question about COMP pin absolute maximum rating.

In the datasheet, COMP to GND = 1.0V to 1.6V.

But I don't know 1V to 1.6V absolute maximum rating. 

Is the operation range 1V to 1.6V?

My customer found 2.1V COMP pin voltage in the customer board at start-up.

So I would like to confirm about the absolute maximum rating of COMP pin.

Best Regards,

Kikuchi

Parents Reply
  • The Abs Max rating is an indicator of the limits to which any pin might be forced from the outside world.  It has most relevance to things like supply pins and input pins, where the customer is potentially driving pins. In the this case, COMP going towards 2V during startup is ok.

Children
No Data