LTC4162-L charging issue

Hello,

Please help me as I'm stuck!

I use LTC4162-L to charge a lithium battery and it works great!. I had a few prototype boards and every time I solder it myself. I've been having issues with the latest boards and the design and layout is the same as previous ones! It gives an output but it doesn't charge the battery. I tried resoldering a few boards multiple times but still haven't fixed it. Sometimes charging turns on but it turns off next time I plug in.

I took the good working board and non charging board and swapped all the components one by one and still good working board worked meaning that there wasn't a component issue.

I tried measuring the voltages around the IC to spot the difference and I noticed that pin 11 is 1.01V for a good working board and pin 11 oscillates from 0V to 2.4V slowly maybe once per second. What does it mean? 

What are the other reasons for this IC not to charge? I use it standalone design without a micro so I can't debug it. Maybe its a thermal issue, I'm not sure.

I resoldered it multiple times now and its the same issue. The output still works even when I plug in the battery. Its just doesn't charge. I had a few times charging while testing so its not like it doesn't work all the time. Also the battery I'm using is low so it should charge. I also tried leaving it for like half an hour.

Thanks!

Regards,

Emilija

Parents Reply Children
  • 0
    •  Analog Employees 
    on Jun 14, 2019 3:14 PM over 1 year ago in reply to SRoa791

    Hello,

    I can't be sure, but it looks like the pad is shorting to all the pins? Probably just a setting in the viewer but worth checking.

    The actual pad looks good, and you properly used vias in the center of the pad to connect the GND.

    The problem here is that your GND plane is choppy due to routing and this will cause noise which may cause the chip to malfunction. I recommend you go to a 4-layer board if possible and copy the demo board layout.

    You might be ok here with your low charge current requirement, but I can't be sure and I would not take the risk.

    Regards,

    Zack

  • Hi, thank you for you answer.

    If it is because of the remoteness of the image but the pad is not short. At this time it is almost impossible to change to a four-layer design. I changed the routing of a single track that is in the bottom layer to see if the noise can improve, what would have to change to be able to use a two layer PCB? Also I have more components in the PCB should I put a ferrite to separate GND?
    Pad number 29 must be soldier?

  • 0
    •  Analog Employees 
    on Jun 18, 2019 3:41 PM over 1 year ago in reply to SRoa791

    Four layers are highly recommended. This may work but I am not confident in the grounding. That is the main concern with a  2-layer PCB, it is very difficult to have good grounding when you are forced to route on both layers.

    That long INTVCC trace makes me nervous. I recommend you put a 100k resistor in series with that trace. See the DC2038A demo board schematic for an explanation why.

    Make sure the GND return path from the 2P5VCC cap is very short in returning back to the GND pad, 29.

    Yes, absolutely pad 29 must be soldered.

    I recommend you review the DC2038A documentation as well as the PCB layout recommendations in the LTC4162 datasheet.

    Regards,

    Zack

  • Hi Zack 

    I was talking to my co-workers and my boss and they said that I can not do the four-layer PCB that I should use two layers. Does Analog have another IC for solar applications for two layers?

    In case that we decide to make the PCB design that I have at this moment, to weld the pad 29 and due to these vias the technique should be applied via pad? This requires a special assembly?

    Regards,

    Sergio Roa

  • 0
    •  Analog Employees 
    on Jun 20, 2019 2:50 PM over 1 year ago in reply to SRoa791

    Hi Sergio,

    It is not really up to the IC, we would recommend 4 layers for any layout in this power range. You can make it work with 2 layers, it just needs extra care. This is probably the best IC for the job.

    I don't know what you mean, but the IC pad 29 needs to be soldered to the PCB and should have vias to a GND plane. There's no special assembly requirement, this is standard for QFN packages.

    Regards,

    Zack