Post Go back to editing

LTC4162-L charging issue

Hello,

Please help me as I'm stuck!

I use LTC4162-L to charge a lithium battery and it works great!. I had a few prototype boards and every time I solder it myself. I've been having issues with the latest boards and the design and layout is the same as previous ones! It gives an output but it doesn't charge the battery. I tried resoldering a few boards multiple times but still haven't fixed it. Sometimes charging turns on but it turns off next time I plug in.

I took the good working board and non charging board and swapped all the components one by one and still good working board worked meaning that there wasn't a component issue.

I tried measuring the voltages around the IC to spot the difference and I noticed that pin 11 is 1.01V for a good working board and pin 11 oscillates from 0V to 2.4V slowly maybe once per second. What does it mean? 

What are the other reasons for this IC not to charge? I use it standalone design without a micro so I can't debug it. Maybe its a thermal issue, I'm not sure.

I resoldered it multiple times now and its the same issue. The output still works even when I plug in the battery. Its just doesn't charge. I had a few times charging while testing so its not like it doesn't work all the time. Also the battery I'm using is low so it should charge. I also tried leaving it for like half an hour.

Thanks!

Regards,

Emilija

Parents
  • Hi Emilija,

    When you say that you swapped all components, do you mean all components besides the LTC4162? If that's the case, I would assume that the non-working unit has been damaged somehow and I would suspect that replacing it with a fresh unit would fix what you are seeing.

    The RT pin should not be oscillating like that for any reason. Is there a valid resistor on it?

    Regards,

    Zack

  • Hi Zack,

    Yes, I swapped all the components including the LTC4261!

    Yes, I have a correct resistor fitted 93.1K. And the exactly same resistor was fitted on the other board.

    I'm going to try a few more times to solder the IC on because I still think its a soldering issue. Maybe my soldering technique is wrong:

    I place the solder paste and the IC. Then I use a hot air set to 210°C. Then I use a soldering iron set to 350°C and go through the long pads to get rid of shorts. My old technique was to just to remove the access soldering with a wick and now I found it easier just to go through with a soldering iron. My old board still works using the new technique.

    I might try the exactly same components I have on a good working board to transfer them to the fresh new board.

    Another option is to design a PCB that connects IC to the micro so I could actually read what's going wrong.

    Please suggest any other ideas.

    Thank you!

    Regards,

    Emilija

Reply
  • Hi Zack,

    Yes, I swapped all the components including the LTC4261!

    Yes, I have a correct resistor fitted 93.1K. And the exactly same resistor was fitted on the other board.

    I'm going to try a few more times to solder the IC on because I still think its a soldering issue. Maybe my soldering technique is wrong:

    I place the solder paste and the IC. Then I use a hot air set to 210°C. Then I use a soldering iron set to 350°C and go through the long pads to get rid of shorts. My old technique was to just to remove the access soldering with a wick and now I found it easier just to go through with a soldering iron. My old board still works using the new technique.

    I might try the exactly same components I have on a good working board to transfer them to the fresh new board.

    Another option is to design a PCB that connects IC to the micro so I could actually read what's going wrong.

    Please suggest any other ideas.

    Thank you!

    Regards,

    Emilija

Children
No Data