Post Go back to editing

DC1237A-A for LTC3527 evaluation

I use DC1237A-A for LTC3527 evaluation and have the SW2 stop problem
would you teach me what happens and how I can fix this problem.
Here are settings in DC1237A-A.
- JP7(VOUT1) to 5V and connect 50ohm load
- JP8(VOUT2) to 3.3V and connect the electronic load(50mA)
- JP4 to 1.2MHz
- JP5(/SHDN1) to EXT
- JP6(/SHDN2) to ON
- JP1 to Parallel and connect Power Source with the setting og 2.4V and current limit 2A
After VOUT2 is regulated, I start up ch1 with /SHDN1.
During VOUT1 raps up, SW2 stops and VOUT1 goes up and down.

scopeshot

Parents Reply Children
No Data