Can LTM8045 be connected in parallel to increase output power?

The input is all 12V, the output needs to be +15V, -15v, +15V is generated by LTM8056, and -15v is generated by LTM8045,  two problems as follow:

1. The power of -15v is not enough. Can the LTM8045 be connected in parallel?

2. The outputs of +15V and -15v are common ground, and both are non-isolated. Is there any output balance or current sharing problem?

Parents Reply Children
No Data