Hello Team;
Could you kindly help on the power request as below; please?
Our basic power management ic requirement for battery based product is as below:
1), the battery will be 3V-12V, actually we need the work range of DC/DC shall between 2V – 12V
2), the efficiency should > 80% in low load current such as 30uA, the maximum output current shall > 600mA better.
3), the output voltage will be 2.5V – 3V, so the DC/DC should be buck-boost type.
4), -40 – 85c work temperature range.
thanks;
Bell