KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
LT3085
Recommended for New Designs
The LT3085 is a 500mA low dropout linear regulator that can be paralleled to increase output current or spread heat on surface mounted boards. Designed...
Datasheet
LT3085 on Analog.com
AD5272
Production
The AD5272 / AD5274 are single-channel, 1024-/256-position digital rheostats that combine industry leading variable resistor performance with nonvolatile...
Datasheet
AD5272 on Analog.com
Hello,
I'm trying to use LT3085 as adjustable current source. From application note it seems to be very easy:

My design is as follows:

AD5272-100 is 100k Ohm resistor controlled through i2c interface.
I have two issues:
1. Output current is not adjustable. It means that current is not changing if I change resistance of AD5272 (for 0Ohm or 100kOhm output current is the same)
2. Changing load in range 2-100Ohm cause that voltage on output is keep stable (~2V) but current is changing so it does not work as current source but as voltage source
Could you please help me with understanding what is wrong here?
Hi,
Could you replace AD5272 with a resistor and check if the current is varrying. This is to verify if the Part LT3085.
Could you share me the screenshots of the Waveform of the I2C transactions
Regards,
Koushik
With a common variable resistor it is working correctly.
Regarding i2c communication, I measured resistance on AD5272-100 for DAC register set to 0 and 1023 and resistance is about 37Ohm and 99.8kOhm respectively thus I think there is no issue with communication. I've noticed that if there is nothing connected to A and W terminal of AD5272 there is about 25mV between A and W, is it expected to have some voltage there? For sure I replaced AD5272 with new one but it did not help at all.
Hello Koushik,
Any ideas why it is not working with AD5272?
Best Regards
Tatery
Hi Tatery,
There might be some stability issues arising due to capacitance of the PINs A and W. You could do the following:
1. Interchange the terminal connected to set pin to W. or
2. Try to follow this scheme to create a current source:

PS: Do you keep the AD5272 powered-up through out the operation?
Regards,
Koushik