Post Go back to editing

Using LTC4015 along with BMS ( Battery Management System)

I have a LiFePo4 battery rated at 25.6 V 30 Ah with max. charge current at 15 A and discharge at 35 A. It is pre-installed with BMS. 

I would like to know if I can use LTC4015 with BMS installed in battery. Will there be any performance issues becasue

Datahseet says LTC4015 has  constant-voltage charging (CC-CV) technique, does it hinders with BMS's CC-CV method of Charging. 

(My sole purpose is to design coulomb counter by connecting to battery externally)

Thank you. 

Parents Reply Children
  • Yes Zack, you're correct. Thank you again.

    Hence I conclude that using :

    1.  RSENSE  (50mV / Imax) , I get RSENSE ≤  1.56 mOhms  ( IMAX = 32 A)

    2. RSENSE ≤ ( 0.340mAh• 2^16   50mΩ )/ QBAT ( For  IMAX = 32 A and Battery Capacity = 30 Ah )                      I get RSENSE  37.13 mOhms 

    Thus, using both equations 1 and 2, RSENSE for my application is 1.5 mOhms 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.