Post Go back to editing

Using LTC4015 along with BMS ( Battery Management System)

I have a LiFePo4 battery rated at 25.6 V 30 Ah with max. charge current at 15 A and discharge at 35 A. It is pre-installed with BMS. 

I would like to know if I can use LTC4015 with BMS installed in battery. Will there be any performance issues becasue

Datahseet says LTC4015 has  constant-voltage charging (CC-CV) technique, does it hinders with BMS's CC-CV method of Charging. 

(My sole purpose is to design coulomb counter by connecting to battery externally)

Thank you. 

Parents Reply Children
  • Hello,

    The 0.340 is in mAh already and your capacity was 30Ah, so if you multiply the 0.340 by 10^-3 to convert mAh to Ah then you should just divide by 30 (Ah) instead of 30,000 (mAh). So either way that would yield 37mOhms.

    Regards,

    Zack

  • Yes Zack, you're correct. Thank you again.

    Hence I conclude that using :

    1.  RSENSE  (50mV / Imax) , I get RSENSE ≤  1.56 mOhms  ( IMAX = 32 A)

    2. RSENSE ≤ ( 0.340mAh• 2^16   50mΩ )/ QBAT ( For  IMAX = 32 A and Battery Capacity = 30 Ah )                      I get RSENSE  37.13 mOhms 

    Thus, using both equations 1 and 2, RSENSE for my application is 1.5 mOhms