LTC3108

Can anyone please give me some help that what is the output current of LTC3108?? & is it continious  in nature or only occurs for a very short period of time?? plzzzzzzzzzzzzzzzzzzzzz help me or give me suggest me some alternative for this to convert 60mV to 3-4 volt with the help of TEC12706??

  • 0
    •  Analog Employees 
    on Mar 26, 2019 4:15 PM

    Hi , 

    The max output current will depend on turns ratio of the selected transformer and TEG specification such as TEG size, TEG source resistance and the differential temperature across the TEG. You can refer Page 4 and Page 5 of the datasheet where you have several graphs for Output current vs Vin for different turns ratio and source resistance. 

    Output current can be continuous but its max current capability will be few hundreds of uA since these energy harvesting parts are designed for very low power applications.

    Thanks