I have managed to communicate successfully with the LTC6811-2 over 4 wire SPI on a custom PCB. However, when I attempt to communicate over isoSPI with a custom PCB that has the LTC6820, I do not get a response from the chip. Below are the schematics for the custom PCB with the 6811
On the board with the LTC6820, this is my schematic -
I get the following signal on the IPA and IMA of the LTC6811 when using a very large timescale of 100ms and voltage scale of 2V-
When I zoom into the rising edge of one of those to a timescale of 50us and 1V I see this-
That is valid data coming from the LTC6820 as far as I am able to discern. The DC 5V pulse followed by a slow decay that I can only assume is happening due to the leakage of the C_IPMA capacitor occurs on both the IPA and IMA lines which results in no pulse being coupled onto the isolated side of the communications
Urgent help would be greatly appreciated
Thanks
Chai
Added tags
[edited by: sindagi2 at 10:35 PM (GMT 0) on 22 Mar 2019]