LTM8063 on DC2494A ev board: PG pin pull-down

Hi everyone,

I am working on a design with the LTM8063 on DC2494 evaluation board. I noticed that the ev board has a 100k pull-up to Vout since the LTM8063 PG is an open collector output. The PG signal goes to an input pin of an ATF1508AS CPLD, which may have 10uA input leakage. On 5V this can be modeled as a 155k resistor to the CPLD 5V.

Now, I want to build in some hardware protection in case the line between the LTM8063 PG and CPLD input goes high impedance. For this I would use a pull-down resistor, but due to the CPLD gate leakage this resistor should be arround 20k max. And that is not compatible with the 100k pull-up on the DC2494 board (a 5V PG signal would arrive as 1V at the CPLD input).Lowering the pull-up resistor on the DC2494 board is an option, the datasheet specifies a 150uA typical sink current on the LTM8063. Does this mean that the pull-up resistor should be min 33k?

Thanks,
Stef



Added schematic image
[edited by: StefVC at 10:12 AM (GMT 0) on 18 Mar 2019]

Top Replies

Parents Reply Children