Post Go back to editing

LT3474 SHDN pin control

Hi, I want to use MCU pin to control SHDN pin of LT3474.

As in the datasheet, I see the LT3474 doesn't have the internal pull down resistor so I must to use external resistor to pull down on the SHDN line, right?

This is a discussion with my colleague and he doesn't want to use external resistor. Please let me know what is correct.

Parents
  • Hello,

    If your MCU can drive its digital outputs high/low you shouldn't need any external resistors on the SHDN pin. Assuming the digital outputs can properly drive the SHDN pin, you should just be able to connect the MCU output directly to SHDN with common grounding between the two devices. The SHDN pin needs greater than 2.65V to enable the part, and less than 0.3V to disable the part. You will need to ensure that your MCU can pull the pin all the way below 0.3V to guarantee shutdown, as well as drive the pin higher than 2.65V to ensure it is turned on. 

Reply
  • Hello,

    If your MCU can drive its digital outputs high/low you shouldn't need any external resistors on the SHDN pin. Assuming the digital outputs can properly drive the SHDN pin, you should just be able to connect the MCU output directly to SHDN with common grounding between the two devices. The SHDN pin needs greater than 2.65V to enable the part, and less than 0.3V to disable the part. You will need to ensure that your MCU can pull the pin all the way below 0.3V to guarantee shutdown, as well as drive the pin higher than 2.65V to ensure it is turned on. 

Children
No Data